[ TPS61175 ] Shutdown Current (Isd) vs Vin
Hi,
Do you have any data/information on the maximu shutdown current (Isd) dependency over input voltage(Vin)?
The datasheet specifies the max shutdown current as 1.5uA under the condition of Vin = 3.6V.If you
I guess if Vin increase, this shutdown current also increase. Do you have any data and/or information?
Specially, it's helpful if you have data for 7V, 8V range.
Thanks,
Ken