This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92515HV: Shunt PWM dimming ratio and Shunt PWM frequency requirement

Part Number: TPS92515HV
Other Parts Discussed in Thread: TPS92640

Hi,

I am comparing TPS92515HV and TPS92640. I dont understand the main reason of different dimming ratio between those 2 parts.

Also, I didnt find out what is the recommended Shunt PWM frequency operation. Is it depend on which FET that I chose? If so, can you give me an example of best case scenario.

Parts Amps Voltage Range Shunt PWM PWM Analog
TPS92515HV 2A 5.5V - 65 V 10000:1 1000:1 200:1
TPS92640 1A 7V - 85V 20000:1 2500:1 500:1

Thanks,