This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27411-G1: bqstudio compatibility inquiry

Part Number: BQ27411-G1
Other Parts Discussed in Thread: BQSTUDIO

Hi TI,

I would like to check the communication status (sbs) and so on by using bqstudio, but I can not confirm it because there is no bq27411 final bqz file.
If it is set to 0421_1_09_A0-bq27411G1C.bqz, which is currently held, an error such as the attachment will occur.

Requests :
1. Request the file 0421_1_09_B0-bq27411G1D.bqz.
2. Please check the version of bqstudio to prevent errors such as attachment when executing bqstudio with 0421_1_09_B0-bq27411G1D.bqz.

Thank you.