Other Parts Discussed in Thread: BQ51051B, BQ51052B,
Hello,
I am working with this device while I have some questions regarding the temperature sense circuit design.
If you look on the datasheet, on Page 8, there are some thresholds in percentage of internal TS bias voltage for different temperature levels, like 0, 10, 45, and 60 Celsius degrees.
I have questions regarding the equations on Page 24, how could you design the %Vhot and %Vcold thresholds?
From I understanding of this, if we say the safe charging temperature range is 0 to 60 Celsius degrees, according to the electrical characteristics on Page 8, the percentage should be typically from 13.1% (60 degrees) to 58.7% (0 degrees), right?
However, I calculated back by the given example on Page 25, and I just found out the %Vcold is 36.424% while %Vhot is 33.169%. This is quite different from the design perhaps.
Therefore, I wonder if we should define the %Vcold and %Vhot, is it free to choose in between 13.1% and 58.7%? I personally doubt a little bit about the correctness of R1 and R3 on Page 25. Would you confirm that please?
Thanks in advance.
Best regards