This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2611: 12V to -12V current limit

Part Number: LM2611


Hi,

I found a difference in specification from the National datasheet to TI datasheet.

Datasheet National : DS200181 January 2005
Page11
12Vin to -12V out => maximum output current is ~180mA

Datasheet TI : SNOS965J –JUNE 2001–REVISED DECEMBER 2015
Page17
12Vin to -12Vout => maximum output current is 400mA.

The switcher goes in shutdown at 85degC with ~150mA load. What is the right specification for -12V output? (180mA or 400mA)

Regards