This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116: Design Review for pulse current output

Part Number: LM5116

Hi,

We have designed one buck converter for following requirement, this supply is having demand of pulse current requirement, any one can review this attached schematic and provide the feedback, my assumptions are compensation network to be adjusted and output capacitor value if anything. 

this design is not working for below pulse current requirement.

Part No: LM5116MH/NOPB

Vin (nominal)=10V

Vout =3.3V

Iout,max= 3.5A

SW frequency: App. 1MHZ.