This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40428: Ambient Temperature Specification

Genius 12865 points
Part Number: TPS40428


Hello Team,

the TPS40428 data sheet specifies the recommended junction temperature range from -40°C to +125°C but there is no information about the recommenced operation temperature.

I assume -40°C to +85°C.

Can you confirm this, please?

Thanks and Best Regards,

Hans

  • It will depend on your operating conditions and PCB design. As an extreme, you can operate at Ta = 125 C. so long as your power dissipation is 0 W. So you will need to calculate your power dissipation and estimate the thermal parameters of your board.

    Ta max = 125 C - Pdiss * Theta J-A