A 5 volts switching regulator feeds the input of the buck-boost TPS63050. When activated to charge a super capacitor of 1.5F, in soft-start mode (PWM), the input goes to 6V with traces of oscillations.
When the soft-start part is over, it ends. I tried to filter the input up to 220uF, without success. The input, through a switch, can come from a lithium battery. The effect is smaller with it.
I would rather not remove the soft start function as the inrush current is limit for the circuit.
Thanks,
Julien Lauzon