On page 21 in section 8.2, Typical Application, Figure 11, Typical Application Circuit, R11 is specified as 2K ohms. In Table 4, Supporting Components for Figure 11, R11 is specified as 2 ohms. What is the correct value?
Again, in the schematic (Figure 11) there is a 0.1 MFD capacitor in the very lower, left corner of the schematic (between the TS pin and ground). It is unlabeled. I suspect this is C1, as C1 does not appear anywhere in the schematic and its value equals Table 4's stated value for C1. Is this correct?