This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Bq34z100-G1 No Ack from device, ev2300 V3.1C

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQSTUDIO, EV2400, BQ34Z100EVM
I have a custom bq34z100-g1 board & EV2300 is not able to read the ckt. I have attached a screenshot.
Earlier I was using EV2300 V3.1C & try to read on ckt. And software is bqstudio V1.3.52. I was getting error "No Ack from Device"
Then I had updated the EV2300 to V3.1m & then I tried to read again the IC, but again error.
Voltage on pins are:
1. REGIN/CE: 4V
2. REG25: 2.5V
What could be error.
1. Did I damaged the IC as mentioned in above link. From starting bq34 was not responding . I havent flash anything. Could it be the reason that on reading bq34 with EV2300 V1.3C can brick it?  But if that would be case then voltages on REG25 will not be 2.5V?
2. Any other reason? 
3. Also please tell how to update EV2300 to latest version.
Is it 3.1m or 3.1r.?
Please attach the updated files.