Other Parts Discussed in Thread: BQSTUDIO, , GPCRB
Hi,
We have some golden images for this gas gauge depending on the used battery (we have 3Ah and 6Ah batteries). We are now using them on some protoptypes. We have noticed a strange behaviour on the state of charge measurement. There are some discontinuities. For example, after using the battery for some operation our prototype had 95% of SOC. Suddendly, it got down to 79%. And then, with no input current, it went up very slowly (it took 6 hours) to 95% again. Other times, the discontinuity is also in when it goes up again. Suddendly we see a 65% value, and then a 90% value. We see that the Full Capacity is also modified in these discontiniuties. But we don't see the reason. We started to think that it could be a temeprature issue, but after registering temperature we saw that sometimes it looked like the full capacity varies with temperature, but sometimes not. So we don't know what could be the reasons to these variations on full capacity, and therefore in state of charge.
We don't do any "Reset" operation to the gas gauge. There could be a "unseal" operation to modify a parameter and then a "Seal" operation when finished. Could this affect?
Could it be possible to have a "bad" golden image?