This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: no cell chemistry data for Sony US18650VC3 cell?

Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: BQSTUDIO

I've just installed the latest cell chemistry update, version 554, into bqStudio. Cannot find the Sony US18650VC3 cell. (It is spec'd as 3.7V, 2000 mAh nominal, 1800 mAh rated) Does T.I. plan to add that one anytime soon? Or can you recommend another cell's chem ID that would be close?