Hi everyone,
Can someone tell me if +5vdc output seems abnormally noisy? Powered by a +24v off line switcher also powering an inductive motor load with 470uf at inverter PCB
The +5 is bucked again by 3v3 LDO (TPS73733) and it seems to cause a 50mv PP ringing on +3v3 that gets into all MCU peripherals.
What should I check for being bad LM5007 circuit, Schottky D5 checks ok on diode check, C46 22uf SMT Panasonic can type electrolytic tests Ok cap checker and 10uf can type at input is newly added.
There is also 3/4 amp series fuse added on PCB after the polarity diode D8. Switcher PCB was part of an RDK, cut off to use with another project.
Capture shows LM5007 idle mode no motor loading +24v.
TPS73733 +3v3 output seem to have a bit to much ring or is this industry acceptable DC?