This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS562200: TPS562200 vs. TPS562209 Psi JB difference

Genius 17165 points
Part Number: TPS562200
Other Parts Discussed in Thread: TPS562209,

Hi all

Looking at the Datasheets I find for the TPS562209 a Psi(JB) of 60.4°C/W and for the TPS562200 one of 13.2°C/W.

As these parts come in the same package and have the same RDSon I wouldn't expect  to see a difference in thermal parameters.

Please comment / clarify.

Best regards

Ue