This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54302: EN pin control using N.O. switch

Part Number: TPS54302


I'd like to turn on the device by closing a Normally Open switch. However, the datasheet specifies that the EN pin needs to be floated to enable (which calls for a Normally Closed switch to pull the EN pin to GND for off, and can then be opened for EN to float).

Can I instead use the UVLO resistor voltage divider circuit as shown on page 10 of the TPS54302 datasheet, but modified to insert the N.O. switch in series with R4? This way, when the switch is open (off), R4 is disconnected from the EN pin. R5 is always connected to EN and will pull down the EN pin to GND, disabling the device. When the switch is closed (on), R4 is connected as per the circuit on page 10 and acts as a divider pulling the EN pin up over the VENrising threshold and enabling the device. 

Would this modification work correctly? Thanks.