To Whom it may concern:
Does TI have a cross reference part for LTC3408EDD (Linear Technology part)?
Thanks
Art
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Art,
Using the XRef tool on TI.com: http://www.ti.com/sitesearch/docs/universalsearch.tsp?searchTerm=LTC3408#linkId=8 , you'll see the LM2738 is a close match (but it is not a direct replacement):
| LTC3408EDD | LM2738 | ACTIVE | 550kHz/1.6MHz 1.5A Step-Down DC-DC Switching Regulator | F: Similar Functionality |
~Leonard
Hi Chris!
We need a direct footprint replacement for the LTC3408EDD with the following requirements:
1). 6V input or higher
2). 600mA ouptut or higher
3). 3V output.
Please let me know if there is a TI part which we can use.
Thanks
Art