This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54061: Input volatge with 50Hz 12Vmin/38Vmax

Part Number: TPS54061

Used circuitry TPS54061 output by webench tool. The input voltage for this design is from a half-wave recifiere and the min/max differ strong. @150mA/3.3V output the max input voltage is 38V, the min voltage is 12V -> input voltage looks like as 50Hz saw tooth voltage. Does this usage makes problems? The application is with 868MHz wirless transmitter so EMI might be critical. I will add also an output filter.

TPS54061 Schematic Prints.pdf