Other Parts Discussed in Thread: TPS92690, TPS92691
Hi there,
I am new to this forum and I had a question about TPS40211
I would like to use this driver to drive a COB LED FV=40.5 to 54 V (FV changes with LED temperature), FI=2.45A. I would like this controller to be %95+ efficient. And I also would like the controller to be a true constancy current booster. I would like to have analog dimming rather that PWM.
the input is from Li-po battery 7s configuration(17.5-29.4V). I also would like to have the ability to drive another LED (51V 1.5A using the same circuit).
I was looking thought the TPS40211 datasheet and I noticed that the datasheet is very comprehensive in the constant voltage configuration. However, there is not much info on the constant current application. There is one diagram 29 on page 23 which shows the circuit but there is not text describing the design process.
There is also another figure 29 on page 33.
I was wondering if there is another IC i can use one which is specifically designed for high power COBs? maybe TPS92690? I could not find anything on webench
with the tps40211 I wanted to use analog dimming circuit similar to this one:
Any help could be greatly appreciated. I am willing to pay any freelance capable of designing and prototyping this circuit. PM me if your interested