I have a few general questions about Figure 19 in the Datasheet, Typical Application:
Given that Q4 and Q5 are the low and high drivers, respectively, what is the purpose of Q3?
What is SYSTEM and how is it intended to be used?
My application is a battery charger for a removable battery pack. The battery pack will be inserted, charged and then removed. The thing that the battery powers will not be connected to the circuit containing the BQ24610. Is is NOT a design objective to be able to power some device with the charging circuit, even if the battery has been removed. Given that, do I need R15, R19, C9, C15 and Q3?
Thanks.