This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2731: Heating/Failing Issues on Start-Up

Expert 3801 points
Part Number: LM2731

Hello Team,

I am working with a customer who is using the LM2731 in their circuit to boost 5Vin to 12Vout. They noticed that they would every now and then have heating issues on their output capacitor, and also have catastrophic failures on the circuit. 

After reviewing the schematic I noticed that their output capacitors did not meet the requirements of the datasheet. 

For the external capacitors they are using a 2.2uF X7R and a 100uF tantalum capacitor in parallel. Since both of these caps are outside of the 4.7uF to 10uF recommended range, could the heat/failing issues be stemming from this?

I was thinking that the heat issue may be related to the ripple current entering the polarized capacitor depending on the cap's max rating, but I am not sure if that would cause failures either.

Any guidance or input would be appreciated here. 

Best Regards, 

JP