Hi, I'm looking to design a DC/DC converter that takes 115V to 165V input and steps it down to 100V, 10A output. Are there any reference designs or application notes I can leverage from?
Or similarly, any suggestions on taking the same input range of 115V to 165V and stepping it down to 100V, 2A output? Plan would be to use 5 of these smaller converters as opposed to the one.
I've been considering using the PWM controller UC1823A in a buck converter topology or even the UCC28700 if possible, but would be fine with using any device that is recommended.
Thanks, - Jim