Hi
I am going to calculate the Cout by Equation(15) and Equation(16). However I do know the unit(voltage[V] or percent[%]) of Vos and Vus at these equations.
In case of the equation(16), the "(Vout*Vos)^2 - Vout^2" will be negative value if the Vos is 0.25V.
How can we estimate the Vos and Vus?
(e.g Vos = 5%? or 5.25V? or 0.25V? @Vout=5V, and Vus=5% and 0.25V?)
Regards,
Koji Hamamoto