Other Parts Discussed in Thread: CC2650
Hello
I want charge my battery at 100mA but the charging current does not exceed 60mA.
In the datasheet there is an inconsistency on the max value of RISET . 8.9K(p7) and 5.9K(p21).
can you help me ?
my configuration
IN = 5V
RILIM = 4.7K
RISET = 8.87K
TD = VSS
TMR = VSS
RTS = 10K
EN1 = 0
EN2 = 1
Thanks