Hello,
Vin: 10,2V to 35V (normally) DC
Vout: 9V DC
Iout max: 1.5A
Iout normally: 100mA
It works fine, no problem with the values.
But I have an special situation:
The power Vin goes down from 10,2 V to Zero in an Emergency Situation:
In this situation I need: Vin = Vout also a bypass.
Has TI a solution for this situation?
A other regulator?