This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022-Q1: Using external clock from a 3.3V Micro

Part Number: LM5022-Q1


Hi,

I am trying to create a pre-boost followed by a buck converter for start stop applications with the C2000. While looking at the datasheet for the LM5022-Q1 I noticed that it says on page 13 that the RT/SYNC pin needs to have a peak voltage level greater than 3.8V. My issue is that the piccolo C2000 processors are 3.3V IOs.

Do you have any examples of someone using a 3.3V FPGA or micro for externally syncing the clock to the LM5022-Q1?

Thanks!

 

John