This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25100: How to set Battery charging current ?

Part Number: BQ25100

Hi, All.

I Design using 'BQ25100' and Polymer Li-on Battery(3.7V / 200mA[1C max] ; I attach a battery spec. file.)

I don't know how to set battery charging current.

I'd like to fast chaging. so, just 250mA? is that possible? or just 200mA? or more than lower 200mA ?

Please, inform me that solution,ASAP. 

Best Regards,

Inho Jeon.

  • Hello,

    current setting method:

    pin function in the datasheet:

    ISET B2 I Programs the fast-charge current setting. External resistor from ISET to VSS defines fast charge current value. Recommended range is 13.5 kΩ (10 mA) to 0.54 kΩ (250 mA).

     

    Setting method and calculation:

    8.3.6 ISET

    An external resistor is used to Program the Output Current (10 to 250 mA) and can be used as a current monitor.

    RISET = KISET ÷ IOUT (1)

    Where:

    IOUT is the desired fast charge current;

    KISET is a gain factor found in the electrical specification

    For greater accuracy at lower currents, part of the sense FET is disabled to give better resolution. Going from

    higher currents to low currents, there is hysteresis and the transition occurs around 50 mA.

    The ISET resistor is short protected and will detect a resistance lower than 420 Ω. The detection requires at

    least 50 mA of output current. If a “short” is detected, then the IC will latch off and can be reset by cycling the

    power or cycling TS pin. The OUT current is internally clamped to a maximum current of 600 mA typical and is

    independent of the ISET short detection circuitry.