Hi, team,
We are using bq24297, because part of the adaptor current is for other use, so we want to limit the input current to be around 1.7A~1.8A. However, register setting doesn't have it, so we have to use external resistor, however, KILM has a very wide range. Here if we use 250ohm,
KILM=395,158A;
KILM=435,1.74A;
KILM=475,1.9A,
If we want to play it safe to set 1.8A when KILM=475, that means most of time we couldn't use the maximum charging current.
Thanks!
不过也是可以的,寄存器配置为2A输入限制