Other Parts Discussed in Thread: BQ40Z50,
Hi,
I have a circuit with bq40z50 that works fine, but now I want to upgrade the circuit with bq40z50-R1. (I have the new circuit with bq40z50-R1 on hand)
I have access to the .gg.csv that has been programmed in bq40z50, so my following questions are;
Q1a. Is is possible to copy the values/data from the old .gg.csv file(from bq40z50) and import them to bq40z50-R1?
If its possible, I am thinking of making a simple script which will import the old .gg.csv file and compare its values/data with a default .gg.csv file created from bq40z50-R1.
It will then update the default .gg.csv file with values from the old .gg.csv file.
(basically, I want to transfer the settings from bq40z50 to bq40z50-R1)
I read that its not recommended to manually modify the .gg.csv file, but instead open the file with notepad or similar program.
Q1b. Can I convert the .gg.csv file to .txt, without adding additional errors?
Q2. If its not recommended doing as proposed in Q1a.,
What is the easiest/recommended way to transfer settings from bq40z50 to bq40z50-R1?
BR David