Hi,
I try to understand when the power good register bit(Reg08[2]) should be high.
In my case, I have tested several alimentations (PC host and wall adapters), and never have I seen this bit high. Usually, I have between 4.8V and 5.2V on VBUS, and the tested wall adapters were able to source between 1.2A to 2.8A to charge the battery.
So with those voltages and currents, according to the point 8.3.1.4.2 of the datasheet, this register should be high.
My question is, what am I missing and what should I look at or modify in order to have the power good high?
Regards,
Maxime Nicolet