Hello,
I'm currently trapped in a weird problem.
When the bq40z50-r1 wakes up after SHUTDOWN, it calculates a wrong FCC, much different from that it calculates if I apply a RESET.
In numbers:
- the 4S1P pack has learned a QMAX of about 3050mAh against a design voltage of 3000mAh.
- the FCC after a RESET is calculated at about 2800mAh (ok)
- the FCC calculated at wake up after SHUTDOWN is alwasy in the range 2100~2200mAh.
I have tried it with LOAD SELECT=7 (default) but also with LOAD SELECT=3, without any sensible difference.
This is quite weird and frustrating, beacause we ship the pack in SHUTDOWN mode and when the users reactivate the packs on first charge they will get incorrect and false perfecption that the pack is depleted
Do you know how to settle this ?
Regards
Pietro