Other Parts Discussed in Thread: TPS28225
Hi, I am building a DC to DC converter using a TPS28226 and 2 N-Channel mosfets. I have been unable to get any response at all from the MOSFET driver. I have gone so far with debugging as to isolate the TPS completely, it is now fed from a 40KHz TTL square wave, VDD is connected to 5V DC (as is the enable pin) I am using a 220nF.. 100nf.. 1nF boot strap capacitor, and have tested with and without a SI7288DP dual N-mosfet with 15V supply. Both gate drive pins remain at zero volts regardless. I have tested with ICs from 2 different supplies, they are all non responsive and I am completely at a loss!