Other Parts Discussed in Thread: UCC21520
Customer strongly inquired CTI (Comparative tracking index) data for UCC27714.
As an example, UCC21520 is specified that CTI is larger than 600V on the datasheet page 6.
Can you send us CPI data or no data?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The UCC27714 is not constructed for electrical isolation, so the mold compound for this device is not certified for CTI index. Per our packaging experts, if certification were done, this compound would likely be able to be certified as > 400 V. This data is provided in good faith to address the customer's inquiry and is not to be interpreted as a specification or guarantee.
If this post has answered your question, please press the "Verify Answer" button below.
Regards,
- Daniel