Part Number: ISO124
Other Parts Discussed in Thread: LM5000, TPS40210
I would like to design a 3-port isolation amplifier with a rated voltage continuous (ac 60 Hz) of 1500Vac across the following ports: Power input to signal input, Signal input to signal output and Power input to signal output. I have selected ISO124 for signal input to output isolation. From the datasheet i found that it is rated for 1500 Vac @ 60 Hz continuous across the isolation barrier.
Iam in the process of selecting a DC-DC converter which can sustain continuous voltage of 1500 Vac @ 60 Hz between its input to output to meet the power to input and power to output isolation for the 3-port amplifier. I kindly request the members to suggest any DC-DC converter (1Watt or 2Watt) with the above mentioned isolation voltage rating to meet the requirement.