Hi ,
I am looking for a Power management IC which can charge a 1C Li Ion/Polymer battery. This IC should receive 3.3V or 5V as regulated input and should give a 3.3V 300mA as output.
This output 3.3v should be driven through the input when input power is present and in absence of it , it should drive from the Li battery.
Please suggest a reference IC part number with an application note.
Thanks
Abhishek