This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS60400: RSWITCH on the datasheet P11

Part Number: TPS60400


Hi all

Would you mind if we ask TPS60400?

RSWITCH on the datasheet P11 shows "resistance of a single MOSFET-switch inside the converter".
We guess that this value will be 12ohm upto 15ohm at 25°C, VI = 5 V.
Do you have characteristic diagram concerned with temparature and VI.
(Our cusutomer would like to know the value in case of  VI = 1.8V, 2.5V, 3.3V, 5.0V with full temapature range(-40 upto 125C).)

Kind regards,

Hirotaka Matsumoto