Other Parts Discussed in Thread: TIDA-00449
We have a problem with balancing FETs getting damaged during the short circuit test. We're using CSD17484F4T FETs with a 33 ohm series resistor and a 5.6V zener from gate to source.
This does not happen every time and when it does it's usually (but not always) the FETs connected to BT1 and BT2. We're using a 7S4P battery with Panasonic NCR18650B cells.
Our design is similar to the one shown in TIDA-00449 for the bq76930 and balancing FETs. All of the filter caps are 220nF and the filter resistors are 1k0. I think everything is within the recommended ranges.
Short circuit current is set to 17.8A with a 100 microsecond delay.
Would putting a TVS across each FET be the most likely solution to this problem? If yes, what current rating would be recommended?
Thanks for your help!
Sheldon