I have questions about protection function of TPS63070.
●short circuit
What is the condition under which short-circuit protection operates?
What are the conditions under which short-circuit protection is canceled?
●Over voltage protection
What is the condition under which Over voltage protection operates?
What are the conditions under which Over voltage protection is canceled?
●Undervoltage Lockout
What is the condition under which Undervoltage Lockout operates?
What are the conditions under which Undervoltage Lockout is canceled?
●Overtemperature Protection
What is the condition under which Overtemperature protection operates?
What are the conditions under which Overtemperature Protection is canceled?
Best regards