Part Number: UCC28910
Other Parts Discussed in Thread: UCC27325, TIDC-CC3200SMARTPLUG
Hi,
I'm having startup issue with the power supply design using UCC28910. The power supply takes 120V AC and outputs +3.3V and -3.3V. I have checked all the soldering joints and component orientation. I tried to remove D8 and it starts, however, the output voltage is not constant. I guessed removing D8 might cause the output voltage to change. If I apply a load that draws 200mA, the output voltage drops from +3.3V to 3V.
I really appreciate if you can help me resolving the issue.
Thanks,