This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ12003: Maximum output capacitance of LMZ12003

Part Number: LMZ12003


Hello there,

I have a customer who is stacking multiple ceramic caps on the output of his LMZ12003 module (he's up to (4) 47uF ceramic caps) and would like to know if there is a maximum capacitance cutoff  that will mess with the internal control loop of the LMZ12003?

Appreciate any feedback you can provide.

-Amanda