Hi,
I have experienced some values changing in the DF of the bq78350 during work.
I would like to validate the DF does not change its static values, I can see there is a ManufacturerAccess() Command 0x0005 - StaticDFSignature.
According to the technical spec it should return the "signature of all static DF" and "The MSB is set to 1 if the calculated signature does not match the signature stored in DF".
1. I am reading with manufacturerData() 2 bytes: first byte 0x25 second byte 0xFD for example - in this case is the first byte the MSB?
2. what kind of checksum is this? if the first byte is reserved?
3. when will the MSB be set to 1? when will it be reset to 0?
Thanks,
Yoav