This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TINA-TI or Spice Models
Can you handle it?
How much it will cost forus?
Hello!
I use the BQ51025 to make a wireless charge for 9 - 10v.
The development board (PWR649A) for BQ51025 uses hole size 0.152mm (6mil) (Figs 1 and 2), but my PCB design company can make hole size only > 0.2mm (8mil). Can I use hole size 0.2 mm? (Figs. 3, 4, 5, 6)
(Fig. 1 - PWR649A)
(Fig. 2 - PWR649A hole size)
(Fig. 4 - footprint from a BQ51025 in my board) - 2d mode
(Fig. 4 - footprint from a BQ51025 in my board) - 3d mode
(Fig. 5 - hole size which I want to use)
(Fig. 6 - SCH)
What happens if I do not connect the SCL&SDA with the ground?