Part Number: LM5005
In operational mode,when the load is open,the test of input current is about 5 mA.
Is it OK?
What is the current when the load is open?
test enviroment: input 12V, output 5V, load open.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The Max Iq on the LM5005 is 5mA, this can be seen in the electrical table of the datasheet.