Hello,
For 17S/24AH, the full charge voltage should be 17*4.2V=71.4v>65.535v, the design capacity=24000mAH<32767,the design energy=17*3.7*24000=1509600mWh.So,voltage and energy is out of range.Please help me to see whether my parameter is right.
1.serial number=17, VOLSET=1, than I calibrate vlotage to 4.2V when I apply 71.2V. Is this right?
2.Then, the design energy= 17s*3.7V*24000mah? Or,the design energy= 1s*3.7V*24000mah? which is correct?
3. Can I set "Design Scale" to any number of 1~10? For example 6, then design energy= 3.7V*24000mAh/6 =14800mwh <32767.
Thanks!