Other Parts Discussed in Thread: BQ27441-G1
Hello everyone,
I have trouble when I want to charge a battery thanks to the BQ24075.
When the battery is connected, it well powers the circuit. It also works well when the USB is plugged but it doesn't charge the battery.
I made several tests at different level of battery charge (20%, 50%, 70%...). I also try to change the value of the resistances, but nothing change: the battery is not charging.
I am using a BQ24075RGTT for the battery management (U7 on the schematic) and a bq27441-g1 for the gauge (U4 on the schematic).
The battery is a Varta 1/LPP 443441 S PCM W.
I am using a USB charger (5v @ 1A).
Does anyone have an idea of what it could come from?
Thank you for your help.
Renan