Hi,
I am an instructor who is trying to teach students to measure solar cell output power using the bq25504. So that they can test out using the different values resistors Roc1, Roc2 OR use an input from a PXI controller. The load in this case is simply a 10k resistor. I have the circuit setup as shown in the image below but I seem to be getting just a constant 50mV output for Vbat regardless of the solar cell. Can anyone help me to where I am going wrong?