This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3701: TPS3701

Part Number: TPS3701

Hello,

have a problem with OUTB, overvoltage detection. Vdd and Vmon are the same, schematic is the same like in datasheet figure 22. Voltage limit is set to ~3.6V by the resistors. Between ~3.6 to 3.8V output is oszillating with ~50kHz, at higher voltage it is stable low. How can I avoid this?
OUTA (low voltage detection) works fine and goes straight to low.

Thank you    Karl

  • Karl,

    What is the input voltage to V_INB? This pin voltage should be 1.7V max and for V_INA as well with the trip voltage at 0.4V. Also, placing a 0.1uF ceramic capacitor close to Vdd is useful if the supply voltage is unstable. The output should not be oscillating due to the built in hysteresis in this device.

    -Michael