This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65131: large ripple at positive output on symmetrical DC-DC converter using TPS65131 in power saving mode

Part Number: TPS65131


Dear All,

I have a customer using the TPS65131 in a split rail application with Vin = 3.6 - 4.2V and Vout = +/-12V.

When using power saving mode, the device shows a very large ripple, which somehow seems to improve by changing the feedforward capacitor.

The large ripple only shows on the positive output, not on the negative.

I do have some more information, but would like to keep it private. Can I have some suggestions as to what is causing this irregular behavior?

Kindest Regards,

Carlos

  • Hello Carlos,

    The ripple in power-save mode is in general higher than in continuous-conduction mode. This is due to the fact that in this mode the device switches only when the output voltage falls below a threshold value: it switches for a few cycles until the correct output voltage is obtained then stops.

    To come back to your specific problem, what is the ripple value you  qualify as "very large ripple"? And what are the loads and output capacitors values?

    You can send me the additional information privately via direct message here or via email.

    Best regards,

    Diaara

  • Hello Carlos,

    Is there any update on this issue?

    Best regards,
    Brigitte
  • Hi Brigitte,thank you for checking on this.

    The device was deemed faulty by the test team, I have sent a query asking for possible causes of the failure and how to mitigate them.