Other Parts Discussed in Thread: TPS2490, LM5069, LM5060, LM5060-Q1
Hello, I am working on a board for automotive (after market) at 12V (nominal).
It will draw around 5-6 A current.
I want to use a protection IC for load dump and over-voltage and I am not sure which is the best for my application.
- TPS2400 looks simple and is cheap but I saw on another thread that it is old and not recommended for such an application (though I would prefer it)
- TPS2490 or LM5060 or LM5069 are other options that I am considering but I am not sure if they are suitable for my application
Thanks,
Mihai