This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51218: TPS51218's output range

Part Number: TPS51218


hi:
  this part just is buck controller, why here have output range 0.7v to 2.6V? customer need 3.3V output, does this part is ok?

many thanks 

  • Hi,

    As I think, the range is set to 0.7~2.6, maybe because the Vinput minimum is 3V, cause the max output limited.
    and actually, I tried 3.3vout@12vin, looks can work normal with different loading.
    but because the designer has left TI, I am not sure if there is other concerns should be taken care of.

    Regards,
    Yuchang