This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28063: UCC28063 gate off condition

Part Number: UCC28063

Hello,

I am designing a 450W / 400V PFC boost converter, using ucc28063. AC input voltage range is 90V to 264V.

When I turn on converter at AC264V, GDA and GDB are turn off for 5ms  like skip mode.

 


 

I've already checked OVP, OCP level.

UCC28063 has another turn off condition? How can I solve this issue?

I'll attach waveforms and test condition.

UCC28063_GATE OFF.pdf